This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22913: TPS22913C反向过流保护设计问题

Part Number: TPS22913


您好!我想咨询,TPS22913C 反向过流保护的机制问题。谢谢~

问题1:如果ON电压为Hi 时,如果出现Vout>Vin>70mV,但是Vout向Vin提供电流的能力有限,只能提供10mA左右的电流,是否会触发反向过流保护功能?

问题2:如果出现Vout>Vin>44mV,ON电压为Hi ,此时Vout电压恢复正常,TPS22913C是否可以立即恢复正常输出?有没有延时?或者会不会输出先跌落然后再恢复正常输出?

问题3:如果出现Vout>Vin>44mV,ON电压从Low变为Hi,此时Vout电压恢复正常,TPS22913C是否可以立即恢复正常输出?有没有延时?或者会不会输出先跌落然后再恢复正常输出?