这个台阶为什么因为VSYS才有的?
是因为VBUS输入5V时,需要限制电流。所以当输出有稳定电压时,才会太高VDDA的电压吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
When IC is powered by 5V (in the second case), VDD voltage is clamped by adapter voltage, until VSYS is brought up. The step is caused by source switch to VSYS.
This is not the case when adapter is >6V, or 20V in the first case, where VDD is always "fully" on.