This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146: LO栅极驱动波形存在震荡,请教该震荡如何消除,是否有什么影响

Part Number: LM5146

根据参考设计进行原理绘制,高低侧MOS管选择DTQ618N10(Qg:19nC,RDS:12mΩ),抓取HO和LO波形,发现LO波形控制MOS关管时存在震荡,不清楚这震荡是否与米勒平台有关系,震荡幅度达到2.33V,MOS的Vgs:1V (min),担心这震荡电压会导致上下管同时导通,存在风险,通过在LO对地并联4.7K电阻能够将震荡电压减小至1.7V,但还是无法消除,请教该风险有多大,有什么较好的策略可以优化吗?目前输出12V正常。