This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16030: LMR16030电源芯片疑问

Part Number: LMR16030


你好,

为了兼容设计,减少芯片种类,LMR16030以下问题请帮忙确认,谢谢!

输入电压:5V-36V , 输出电压:1.8V, 输出最大电流:0.2A, 平均电流:10mA

转换频率500Khz, 电感使用:22uH,  1.15A

问题说明

1、LMR16030是否支持当前电压范围内输出低压和低电流,长时间运行是否稳定可靠?

2、当前选择转换频率和电感值是否合适?