This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B7701-Q1: TPS7B7701 关于SENSE,ERR等引脚功能的疑问。

Part Number: TPS7B7701-Q1

1.SENSE_EN (PIN 8)低激活,激活后SENSE 具有输出电压的能力,用于监测VCC_5V_ANT电压的意思嘛。

2.sense 作为输出pin,激活后不使用有何影响。另外如果用于检测电压,直接从7701的输出端,负载端去采样不是更好嘛,这个工作的作用是什么。

3.ERR作为故障指示pin,这个故障在哪里有说明具体哪些故障。

4,如下原理图设计是否OK.

  • 问题1和问题2在datasheet里找到了,还请帮忙回答问题3和4.

    另外ERR的上拉使用7701的输出5V电压是否OK.在不考虑对端MCU IO耐压的情况下。这种逻辑是否可行。

  • Hi

        问题3, 可以看datasheet 第十二页表 1. Fault Table,  具体说明你可以看对应的FAILURE MODE(在datasheet上找对应说明)。

        问题4,典型应用参考datasheet第十五页,参数选择参照datasheet 第十六页,第十七页。

        在不考虑对端MCU IO耐压的情况下,ERR的上拉使用7701的输出5V电压OK.