This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9222后接两路UCD7242无输出

Other Parts Discussed in Thread: UCD9222, UCD7242

新设计的板卡用一片UCD9222控制两路UCD7242,分别输出CVDD和0.95V,两路UCD7242分别都并联输出,保证每一路都有大于10A的输出能力。通过PMBUS连接到UCD9222后下载离线设计的配置文件到9222上,没有输出。这里附上monitor监测的输出,没有出现fault,但是“output off”这个状态该怎么清除呢?我确认过两路输出的EN引脚已经被拉高了。我把配置文件也随附上,希望有高人能够解答!

配置文件和截图.rar
  • 请问你这个问题解决了吗?

    另外,我想问一下,怎么下载配置文件到UCD9222呢?我的GUI无法导出x0文件,低版本的GUI可以导出x0,但需要密码,不知道你能否提供。高版本的GUI没有导出x0的选项,不知道下载到UCD9222的是哪一个软件,能否详细说一下,十分谢谢!

  • 楼主,我和你的问题一样。也是电压和PWM脉冲都没有输出,不知道您现在问题解决了没有,能否将您的调试情况互相沟通一下,谢谢您!