BQ24295充电芯片,与电池连接后,有2.2mA的漏电,怎么解决。电路原理图下图,图中J20位置连接电池,在没有充电的情况下(即J21管脚没有连接外部5V电源),系统也关闭了,即BAT+位置没有连接负载,设计测试时,把负载都那掉了,就是下图单一的电路。I2C上没有做任何配置。用万用表串联在电池正极与J20-PIN1脚上(即下图BAT+)上,发现电池有2.2mA的电流。按照数据手册,不充电情况下,应该是uA级的电流。这个有没有哪位用过这个芯片,大家是怎么解决的。如果是mA级别,这个漏电太大了,电池在关机情况下就消耗太多了。