This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28063: 1000W电源PFC驱动波形异常

Part Number: UCC28063


1000W电源,输入120-277Vac,PFC输出电压430Vdc,控制芯片使用UCC28063,芯片供电为17V,外围参数通过计算表格得到,电源可以正常工作,驱动信号采用图腾柱形式,单路并联两个MOS,发现其中一路的驱动信号的幅值比另一路高接近2V,详见下图,波形看着怪怪的,不影响正常工作,效率也没受影响。不知道驱动信号为什么是这样,会有什么影响吗?另外720W同规格的电源没有这样的问题。