1000W电源,输入120-277Vac,PFC输出电压430Vdc,控制芯片使用UCC28063,芯片供电为17V,外围参数通过计算表格得到,电源可以正常工作,驱动信号采用图腾柱形式,单路并联两个MOS,发现其中一路的驱动信号的幅值比另一路高接近2V,详见下图,波形看着怪怪的,不影响正常工作,效率也没受影响。不知道驱动信号为什么是这样,会有什么影响吗?另外720W同规格的电源没有这样的问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
更换芯片看看?
驱动电压来自芯片。如果芯片没有再确认一下MOS(只是MOS影响驱动电压,看起来可能性不大)
HI
更换芯片后确认不是芯片问题,将1000w下降到720w, 驱动会正常吗?
从datasheet 第14页的芯片框架图看驱动供电来自芯片内部的LDO输出13.5V, 所以驱动输出高电平应该只与芯片有关。如果确认芯片没有问题,确认一下连个MOS的GND是否存在压差?