This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM365R6: TPSM365R6FRDNR Unstable

Part Number: TPSM365R6


We are using the TPSM365R6FRDNR variant to get +12V like below.


However, I am testing the output of TPSM365R6 power supply
and sometimes the output is +5V but the expected one should be +12V.
It seems that the output voltage is normal when the Input voltage is below 15V and not above it.
We add the Cff capacitor following the datasheet, it is more stable but each time it gets 15V input above, it fails and the output jumped down to 5V around.