Part Number: LM5030
Other Parts Discussed in Thread: TIDA-01352
原理图参考TIDA-01352模块,下图是原理图,变压器是自己设计的匝数比1:2,输入24V,输出48V,90W,目前D1,D2整流后并非是48V,是一组方波,帮忙看一下是什么问题,是原理设计问题还是说变压器其他问题

变压器后端,D1D2前端两路电源也是大小不一致的

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5030
Other Parts Discussed in Thread: TIDA-01352
原理图参考TIDA-01352模块,下图是原理图,变压器是自己设计的匝数比1:2,输入24V,输出48V,90W,目前D1,D2整流后并非是48V,是一组方波,帮忙看一下是什么问题,是原理设计问题还是说变压器其他问题

变压器后端,D1D2前端两路电源也是大小不一致的

Hi
电路完全参照TIDA-01352吗(仅仅更改变压器匝比)? 初级感量等参数有改动吗?
Hi
变压器的设计牵涉到输入输出电压,负载,需要更加这些参数计算变压器的匝比以及感量,因为你的设计相对参考设计很多参数不同,你除了修改变压器参数,还是修改反馈等等。
HI
参考TIDA-01352, 如果仅仅只是修改变压器匝比,是这样吗? 如果是很可能造成上述问题。
如上所说,建议你按照参数重新设计变压器,并确认一下反馈。