This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28740: 关于文档TIDM249的12V应用的问题,在LN之间加10VDC时,CS的1.96R电阻熔断。

Part Number: UCC28740


我按TI的文档TIDM249搭建了如下电路,

起初,给L和N加50VAC时,输出端(12Vdc)没有输出。

随后,给L和N加10VDC时,电阻R19R20因为大电流(3A)烧断。

我试着查找了我的原理图和TIDM249的不同,没有发现不同。

所以我想是不是我忽略了其他什么。

我给LN加1VDC,UCC28740的HV有电压0.4VDC,VDD,CS,FB为0VDC,Q1的pin3对PGND 电压0.4VDC。

我给LN加2VDC,功耗显示12mA,UCC28740的HV有电压0.6VDC,VDD的电压0.1VDC,CS,FB的电压0VDC,Q1的pin3对PGND 电压0.6VDC。

我还应该测量哪里么?

请原谅,我第一次接触这种电路,实在是没有思路。