Other Parts Discussed in Thread: BQSTUDIO
你好,我们有用两种电芯在R5固件基础上做电池包的电量学习,学习后(update status=0e)都有注意到其中两个寄存器的状态位和R2的学习后的状态位不一样:LStaus中CF1:CF0以前R2学习完后是0:0,用R5学习后为1:0.请问是什么原因导致不能变成0:0?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前R2学习后这两位读到的是00。现在R5学习后读到的是10
您好,请参考下面内容:
Both firmware version (R2 and R5) have the same definitions and operation of the CF0, CF1 flags.
Please provide the BQStudio logs showing the difference. The only thing changed is the BQZ file with the R5 firmware, the LStatus register display was changed in BQStudio, operation in gauge firmware is the same.
AL-2162-20230822--.gg.csv这边有用两种电芯,在4串、3串上用R5固件做过学习,学完后也是CF1为1,附件为学习后的gg文件,请帮忙分析,谢谢!
您好,需要学习时的log数据,SREC文件不能看出上面提到的CF0, CF1 旗标的变化过程。