This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24045: BQ24045充电指示异常

Part Number: BQ24045


条件设置:120mAh 锂电池 充电电流设置为:120mA,R_ISET = 4.7KΩ,R_PRE-TERM  = 2KΩ

  现象:1C锂电池充电,充电到4.2V以上,一直处于涓流状态,冲了24小时以上充电指示灯CHG红灯一直常亮

需要协助分析原因