各位专家:
我使用的是5V转±5V,按照手册说明,输出纹波可达±2mV以下,实际测试发现如下:



求指导
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
输出就一个2.2uF陶瓷电容即可,而且不需要额外增加LC.
LM27762本身内部自带LDO, 输出纹波也就2mV左右。(所以不需要额外增加LC)。