Hello TI team
I encountered several problems during the testing process. The first is that the chip will have abnormal waveforms when operating at 300kHz, and the gate oscillation is obvious. The second is that the maximum load current 20A cannot be reached. The last one is the intermittent rest of the chip when it is unloaded.
Hope you can give some good solutions, thank you very much.