想请教一下BQ76930是否有充电检测功能,如果没有是不是与之配合的BQ78350具备这个功能?能不能给讲解一下bq76830在欠压保护后是如何进行充电器检测的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ76930有这个功能,但是保护恢复需要外部控制,结合BQ78350就能自动根据设定的值进行恢复。
这类低侧的保护一般的充电器检测是通过PACK-的电压来判断的,当保护时PACK-和CELL-之间断开,如果插上充电器,那么会在PACK-看到一个相对CELL-为负的电压,通过这个判断的。
按您说的BQ76930具备充电器检测,具体体现是不是通过SYS_CTRL1寄存器中的[LOAD_PRESENT]位体现?我现在的方案是MCU+BQ76930,MCU通过读取[LOAD_PRESENT]位状态就能够判断充电器是否插入吗?如果还需要其他条件,您能否给点建议?
我是通过一个模拟输入pin检测充电器id 输入电压实现这个功能的