Other Parts Discussed in Thread: TPS61232, MC33063A, TPS61230
tps61232带载输出的问题
tps61232输出5.0V然后接mc33063a输出2.5V,然后接20欧电阻,这时tps61232输出只有3.6V的样子,mc33063a输出还是2.5V
tps61232输出5.0V然后接mc33063a输出-2.5V,然后接20欧电阻,启动后,电感出现电流声,tps61232输出和mc33063a输出都不正常,只有1.8V的样子。这时断掉20电阻,输出又恢复正常。在接上20欧电阻,输出同样正常。总之,当tps61232接反向DCDC后带载输出会不能启动。
tps61232接一路mc33063a,一路LDO 3.3V输出,然后接20欧电阻,启动同样输出不正常,都只有1.8V的样子
请问这是怎么造成的?
被TPS61232搞了好几天了,完全输出电流达不到2.1A嘛