Other Parts Discussed in Thread: BQ40Z50
目前遇到一个2S电池使用BQ40Z50R1电量计时(基于BQ40Z50参考线路来描述),电池充满电后,电芯电压为8.66V(即Q2 MOS管S级电压),可是电池Pack输出端电压为11.5V(即Q3 MOS管S级电压),
此时量测到Q2 MOS管的S级电压为8.66V(即电芯电压),Q2 MOS管G电压为Low,此Q2 MOS是关闭的,D级电压与Q3 管D级电压一样11.5V;
Q3 MOS管的S级电压为11.5V(即电池Pack电压),Q3 MOS管G电压为高20V,此Q3 MOS打开,导致D级电压和S级都为11.5V左右电压;想请教这个Pack电压高于电芯电压是否合理?
我的理解:Q2是充电控制MOS,当电池电量充满后BQ40Z50就会控制Pin31:CHG信号拉Low,关闭Q2 MOS管;
Q2和Q3是NMOS,(NMOS的内部PN管是S级到D级),PN结作用,所以S级电压减去PN结电压就等于D级电压,即8.66-0.3=8.36V;
Q2管与Q3管的D级相连的,这样Q3 D级电压就等于Q2管D级电压8.36V,
由于Q3 MOS管G级连接BQ40Z50的Pin28 DSG信号,Pin28是MOS驱动电压20V左右,高电平,
这时Q3 MOS管各Pin脚电压状况:D级=8.36V,G级=20V,S级=0V,此时Q3 NMOS打开,D级电压=S级电压=8.36V