This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
测试时,发现bq4050 shutdown,重新充电唤醒后,电量的rsoc和remain capacity不是shutdown之前的值,而都是默认变为99%。如何才以能保持shutdown之前的rsoc或remain capacity值?
详细的操作如下:
step1:电池实际电量为rsoc=80%,remain capacity=3000mAh (电池容量为3750mAh);
step2:此时对bq4050进行shutdown;
step3:重新对bq4050进行充电,此时rsoc=99%,remain capacity = 3700mAh;
另外,发现reset命令,也有以上现象。