Other Parts Discussed in Thread: BQ24050
充电芯片我选择的是BQ24050,电路设置最大充电电流是100mA,我连接2个万用表,一个观察电池两端电压,一个观察电流,上电发现电压4.2V,电流25mA,冲了一会电后,断开,然后继续冲,发现充电电流从13mA暴降到0.5mA,电压纹波从+-20mV涨到+-200mV。
再问一下怎么来估算电池的电量。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ24050
充电芯片我选择的是BQ24050,电路设置最大充电电流是100mA,我连接2个万用表,一个观察电池两端电压,一个观察电流,上电发现电压4.2V,电流25mA,冲了一会电后,断开,然后继续冲,发现充电电流从13mA暴降到0.5mA,电压纹波从+-20mV涨到+-200mV。
再问一下怎么来估算电池的电量。
对于电量检测功能的需求,请选择对应的fuel gauge器件,请参考TI 电量管理列表,根据电芯类型 器件位置 串联数目等进行选择,以上谢谢!
截止门限电流不知道怎么设置,只能设置充电电流,即使是电池刚冲,再拔掉,效果依然是这样。小于截止门限电流这个除非再加一颗电量测量芯片才可,BQ24050没有检测电流管脚。