This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LM3405驱动LED的问题

Other Parts Discussed in Thread: LM3405, LM3405A

                   楼主 想使用LM3405,想在输入只有4.5~5V的情况下,驱动两个串联的1W LED,但是不知道是否能够实现,所以发帖求助:请教各位高手,使用LM3405,在输入只有4.5~5V的情况下,能驱动两个串联的1W LED吗,每个LED的压降为3.2V左右,每个LED的电流在350ma左右,串联的话就是6.4V,700ma,如果能驱动的话,请问是使用datasheet上的哪个电路例子呢?我每个都试了一下,好像都驱动不了,上电后两个LED闪一下就不亮了。

帖子链接:http://www.deyisupport.com/question_answer/analog/led_lighting/f/76/t/75032.aspx

            对于使用的问题,楼主同样做出了补充的说明:我的电源并不是电池,是外部的4.5~5V直流电,LED是串联的,因为我看应用文档AN1685,上面写着LM3405可被配置为升压转换电路,3V~22V都能支持,能驱动3个串联的LED,但是我使用该电路却没办法驱动我两个串联的LED

             TI FAE:解答了楼主的疑问,明确指出,LM3405只能实现降压电路,对于LED的串联使用是无法实现的,如下图所示:

         那么LM3405究竟是一款什么样子的芯片呢,我们使用LM3405该如何去实现LED驱动电路的设计呢,下面我们就一起去看看TI的规格书,顺便一起了解一下LM3405的驱动电源该如何去设计,如下图所示,是LM3405的典型封装结构图:

           从上面LM3405的典型封装结构图中,我们可以看到LM3405的封装结构是典型的SOT封装,只有6PIN,整体的外观结构是非常简洁的,这样的话,设计起来也可以说是方便很多了,那么LM3405的典型的应用参数是什么样子的,我们一起去看看,如下图所示的列表:

                从上面LM3405的典型的应用参数我们可以看到,LM3405的输入电压范围是从3V到15V,输出电压范围是从0.2V到13.5V。输出电压明显的低于输入电压范围,还有一点更为重要的就是,LM3405的控制结构是典型的BUCK拓扑。也即是说,LM3405只能实现降压输出,楼主所想实现的输出电压高于输入电压范围的设计是无法实现的。那么也就是只能驱动一个LED了。我们再来看看LM3405的典型的应用电路,如下图所示:

         很明显这个是一个BUCK的拓扑结构,其中LM3405的开关管集成在LM3405的内部了,外部电路的设计知识需要一个功率电感,和一个续流二极管,以及相应的输入输出电容就可以了,设计起来还是相当的简洁的。只是需要注意相关部分的元器件的设计问题了。看看内部框图:

           LM3405的另外两种应用电路如下:

        只是BOOST电容充电的方法不太一样,也是无法实现输出升压的:

           我们再来看看LM3405的相关的测试波形,刚开机的时候的波形,如下图所示:

          

           LM3405的PWM调光波形如下所示:

          PWM调光的曲线如下图所示:

       最后还有LM3405的输出电感的设计方法,如下图所示:

          以上就是关于LM3405的LED的驱动电路的设计方法,不过都是降压的线路,这个无法实现升压,与大家分享一下。

  • 由于LM3405只能实现降压输出,所以无法满足楼主的两个LED串联的方案,如果想LED并联使用的话,就必须考虑均流的问题了,设计起来就有些复杂了。这个可以考虑其他的升压方案了。

  • 对于LM3405的设计,TI 还提供了演示版可以供我们设计参考,这个演示版的主要功能:LM3405A演示板采用恒流降压型转换器LM3405A,配置成可驱动一串正向电流为1A的高功率、高亮度LED(发光二极管)的系统。演示板可接受的最大输入操作电压范围为3V到22V。

  • LM3405A演示板的电路图如下所示,大家如果有需要的话,可以直接使用,或者用作功能的测试和验证,关于演示版的详细的技术资料,可以直接参考TI的文档,链接如下:http://www.ti.com.cn/cn/lit/an/zhca321/zhca321.pdf