Part Number: LM51231-Q1

我想要输入5V,输出36V,0.5A,根据TI的电源设计工具,两个反馈电阻分别是14K,和21K,但输出只有12V,怎么回事?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
电路参照webench没有问题,电压升不上去,建议你确认功率电感饱和电流足够大,其次就是确认一下电流保护是否会提前保护,最后layout上确认一下功率回路尽量小。
Hi
你要看一下功率守恒,5V输出,限流是0.5A和1A, 也就是输入功率只有2.5W, 或者5W, 而你的最大输出是12V/4A也就是48W, 肯定是有问题的。如果要做12V输出,只能带轻载。
Hi
确认功率电感饱和电流是否足够大?
layout上确认输入电容尽量靠近,sense电阻,电感输入端。电流保护电阻不能错件,以及layout上避免noise。