帖子题目:BQ34Z100量产文件下载
具体问题:社区会员John Yang1在2013年10月22日,在电池管理板块针对TI的充电管理芯片BQ34Z100量产的问题提出了相关的疑问,请教可否用EV2300下载量产文件,怎么下载?看了下列文档,要生成*.ROM文件,但是在评估软件中未发现此项。
Final Steps Before Exporting bqTester Binary Data-Flash Image (*.ROM File)
1. Start the EV Software for the bq20zxx.
2. Enter the Data Flash window, and push the Read Flash button.
3. In the File menu, click Export, and choose a *.gg filename for saving the pre-learned defaults,
optimized.gg.
4. Open the saved file in a text editor such as Notepad, and change the value of Update Status
to 02, which indicates that the parameters are learned but IT is disabled (as it should be in
before calibration). Also, the cycle number in the SBS Configuration can be changed to 0.
5. Write a .senc file with the correct chemical ID to clear the hidden data-flash constants.
6. Write the gg file that you have modified back into the device.
7. You are now ready to export the data-flash image (*.ROM) file to be used in production.
帖子链接:
http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/47193.aspx
积极参与的TI FAE: Sheldon Cai
从这个案子中我学到的东西:从这个案子中我根据相关的芯片,在TI的官方网站上找到了相关的资料,在这里(www.ti.com.cn/.../ BQ34Z100),我找到了相关的User's guide,通过自己的研究发现德州仪器 (TI) BQ34Z100是一款非常优秀的电源管理芯片,在具体应用中,
Q:请教可否用EV2300下载量产文件,怎么下载?还有gg文件和senc文件具体作用是什么?
A:
不考虑效率的话小批量是可以用senc文件下载的。
Senc包含了固件和全部参数,GG文件只有公开的参数。一般调试时GG文件和记录的充放电数据有比较大的参考意义。senc则用于调试开发阶段的firmware更新,golden 文件导出等。
示例图
下载地址
安装步骤
周期盘点 GG 文件使用记事本中修改
EV 软件 Pro 屏幕
. Data Flash Reader Screen
bqTester 主窗口
bqTester 主窗口解锁
全局配置窗口
VTI 配置框