This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25762-Q1: TPS25762-Q1 Output

Part Number: TPS25762-Q1


hi E2E teams

我使用TPS25762进行PD输出电源设计。

目前通过GUI配置生成“FULL FLASH IMAGE”后通过I2C烧录器将.bin文件烧录进EEPROM后焊接到板上。

然后通过PD诱骗器进行测试,目前可以输出5V和9V,但是12V、15V及20V无法输出,PD诱骗器请求12V或更高电压时,输出电压一直跳动,0V、5V,40V等。

PD诱骗器接在其他成品PD充电器上可以正常输出需求的电压。

我上传了我的原理图,请帮忙检查是什么原因导致的,十分感谢!

TPS25762_SCH.pdf