你好,请问:
1.无线接收器bq51013和bq51003有什么区别?
2.用这两款接收器的话还需要接电源管理模块么?还是说可以直接接电池了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. BQ51013是5W, bq51003则是2.5W。
2. 这两个只是出5V. BQ51050的话是内部包含线性charger的
就是说BQ51013和BQ51003还得接charger再接电池,而BQ5105X可以直接接电池了什么?
您好,针对的应用场合不一样。
系统有些本来就有一个charger的,就不需要无线充电芯片带charger。
如果系统的充电方式只有无线充电这一种,那么可以考虑集成charger的无线充电。
Jason 您好,我想咨询一下BQ51050只有一个CHG脚判断是否正在充电,那么是否充电完成靠什么来判断?