This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于UCC28070A设计应用问题,望回复。感谢!

Other Parts Discussed in Thread: UCC28070A, LM358, UCC28070

1. 电感输出电流为零的区域太大(零点交越失真),降低了功率因数,是否是因为UCC28070A的5PIN检测电压低于0.75V后,芯片就减少或者停止了PWM输出?

 

2.软启动时间tss设置多少比较合适?(100ms~300ms)

 

3.电感选择和计算的理论值差别较大,请问我们如果计算出电感量为150uH,实际选用大概需要多大余量,选择350 uH还是500 uH,甚至更大的? 如果使用共模电感,有什么需要注意的问题?

 

4. 规格书推荐电流检测变压器匝数比NCT 取50~200之间,NCT小于50会影响什么功率因数?我们用的是毫欧电阻采样检测,另外加了LM358运算放大器,将电流检测电压放大了12倍,请问这个放大倍数是否合理,应该在50~200之间吗?没有用电流变压器,是否有影响?

5.RSYNTH 15K~750KΩ推荐该工作条件的理由?超出范围值时应该怎么处理?

6.Gm设为70μs的依据?

7.

Gmc固定为100μs的理由?该值是CT的结合电导值,不论CT TYIPE、(HOLE CT、鉄芯CORE CT)都固定为100μs可以吗?磁气结合的影响有没有?

8.

电流检出方式适用SHUNT方式时,fcxo的计算公式虽然不同但是选用gmc =100μs

    这个常数合适吗?

    公式代入好像不成立,UCC28070应用上从数学思维来看有点奇怪。该计算公式请说明一下其依据。(传递函数近似式)其提示其换算式用于确认。

9.UCC28070有电流反馈,电压反馈功能。本手册中分别有GAIN,位相进行补偿,会不会存在互相干涉(共振)的问题?

10.Rzc的计算公式中⊿ILB部分其计算时乘以0.3这个值,其依据是什么?

11.

本手册中抖动幅度解释说明是fPWM的2/10。

      抖动速率则是fPWM的±10%。

  该功能针对的是高谐波对策、不应该按照EMI Filter常数进行检讨吗?

  会不会使高谐波NOISE恶化?