我现在的客户要我推荐两个型号,一个是能测47maH的电池的电量计芯片,另外一个是可以对3节锂电充电的充电芯片(但输入只有12V)。我翻了一下TI的产品,没有找到满足要求的,各位能给推荐合适的型号吗,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,你的47mah的电芯是什么化学类型的?多少节串联?
如果一定需要精确的电量管理功能,而又没有合适的chem id去选择BQ40Z60这样的器件,那么只能选择BQ26231这样的库仑计了。
12V输入 对应3节串联的电芯,如果是一般的锂电芯,即满充电压为16.8V的,那么不用考虑buck-boost电路,除了一些能量收集的充电器会有升压功能,大部分的充电器本身只是buck或LDO这样的降压充电器,那么此时需要加一级boost电路,再选择一个针对3节锂电池串联的充电器。
TI也有带MPPT的太阳能充电器,如果可以,麻烦楼主告知输入源是一个什么装置以及输出规格。谢谢!
装置是一个小型净化器,因为要驱动一个12V的风扇,所以选用了3cell锂聚合物电池(满电12.6V)配合15V适配器来充电。考虑到电池电压为了驱动电扇就得选用一个能输出12V的buck-boost电路。不过我没有找到满足要求的芯片,所以就建议客户用12V适配器器2cell电池,把电池电压升到12V,不知道这样效率是否有问题?