This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: 电池刚充满电的电压为90%左右,放置一段时间后进行飞行,飞行前显示电量为97%左右,为什么放置一段时间后电量百分比反而变高了呢?百分比由bq40zx0_read_soc(&_battery.soc);获得。

Part Number: BQ40Z50-R1


赛能A电池:放电至15%, 17:19开始用车充充电,18:20左右断充,充电时长约为1时01分,电压为17.4V, APP内显示电量91%,再用AC充电器充至断充,电压为17.39V, APP内显示电量91%
赛能B电池:放电至15%,17:17开始用AC充电器充电,18:07左右断充,充电时长约为50分钟(断电时未充满,三格常亮,一格快闪),电压为17.62V, APP内显示电量83%,再用车充充至断充,电压为17.45V, APP内显示电量90%
赛能A电池:起飞APP显示电量97%,放电至56%,因天气原因降落,悬停续航时间约为12分37秒,天气正常后复飞,放电至10%,总悬停续航时长约为25分 44秒
赛能B电池:起飞APP显示电量 98%,放电至10%,悬停续航时间约为26分46秒

如何能让显示电量差距不能太大?