This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
推荐一款电池充电电路,电池满电压为4,8V,充电器的为7v,1A。
您好,电池满电压4.8V? 您的电池是什么化学类型的,多少节串并联,容量是多少呢?谢谢。
请问你是四节镍氢电池么?容量如何?
四节镍氢电池串联,每节电池为1.2V,900MAH,多谢了
4节镍氢电池串联。每节电池为1.2V,800MAH。
可以使用BQ2002设计符合你要求的充电器,4节镍氢电池充满该是5.6V的吧,你的电池是什么型号的?