我用lm2623设计了一个1.2V升压至3.3V的电路,采用的是lm2623文档里的电路,可是发现启动电压要1.5V才行,但文档里明明写着最大启动电压1.1V。我试着换了频率调节电阻和那个4.7pf的电容,发现当电阻从原来的150k增大到300k时启动电压降至1.4V,但还是不能满足我1.2V的要求。我以前也用lm2623设计过电路,那时用150k的电阻和4.7pf就能正常工作,不知道是怎么回事?可以排除焊接和元件本身的问题,因为焊了三块除了一样的问题,而用的外围部件都是上次用过的,上次没有问题。