This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的TI工程师,您好:
①我想选型一款DCDC模块,输入为+24V左右,需要输出一个-18V@2A的低纹波输出,在负电压输出的器件选型上我在webench上看到了一款比较合适的型号LM5116MH/NOPB,推荐的设计原理图如图,如果照此严格设计是否可行或者有其它推荐的简单设计能满足性能的正电压输入负电压输出型DCDC,谢谢!
②或者推荐一款能够输入+24V左右,能同时输出-18V@2A和+18V@2A的双路输出模块,谢谢!
Hi
可以的。
或者选择输入电压大于42V, 负载能力大于2/(1-18/42)=3.5A的其他降压芯片也都是可以的。
采用上述LM5116之类的同步芯片效率会较高一些,电路相对复杂一点。
也可以选择TPS54560之类的非同步芯片,电路简单点。
Hi
谢谢您的推荐。TPS54560外围电路简单比较适合,负电压的参考设计是否能完全借鉴TPS5430的应该这样类型的电源芯片负电压都是这样的设计的吧?连接是否是https://www.ti.com.cn/cn/lit/an/slva257a/slva257a.pdf 谢谢!
如果我还想通过在接一级稳压的话是否可以考虑使用LDO芯片比如LM1086,但是如果是压差在3V,需要输出1A左右,根据手册大概算出来它的常温下的结温在25+3×1×40.8=147.4° 我同时看到通过PCB开窗增大铺铜设计能够使得θJA降到20℃/W左右,但是这个图参数没有指明是几层板,如果我是四层板上下开窗是否降温效果会更好,或者有更好的非DIP封装,散热更强的LDO推荐
Hi
选择LDO, 如果电流较大如1A, 就要确认尽量减小输入输出压差,否者功耗会很大造成芯片温度特别高。
要做负压转换,是能选择负压输入的LDO.
TPS7A4501KTTR输入输出能支持-±20区间的输入输出,那就是说支持负电压输入,负电压输出,我想请教一下TPS7A4501KTTR具体应该怎么样设计负输出电路,是和输入输出都为正电压一样的设计吗,谢谢