This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730: 问题如下:

Part Number: BQ25730
Other Parts Discussed in Thread: BQ24650, BQ25756

各位专家

     您们好,我们有个 需求,需要实现 对 铅晶(胶体)电池的充放电管理,及负载的供电和路径管理

     电池是12V两节串联,输出电压24V,充电电流5A的。

     之前有看了一下 BQ25730,是带路径管理,但是电池电压是到23V的。如果给24V的电池充电,能满足要求吗。 

     另外我这边 BQ24650电池电压能到26V,但是没有路径管理。要满足路径管理的需求,需要怎么样的电路设计呢?

     

     电池特性:

      1、铅晶蓄电池低温充放临界温度是-40℃,不同低温环境下的充放电容量即SOC分别是:

           -10℃时以0.15C恒压2.54V/单体充电14h,再次放电容量为额定容量的80%-20℃时以0.15C恒压2.58V/单体充电16h

           再次放电容量为额定容量的65%-30℃时以0.15C恒压2.62V/单体充电18h,再次放电容量为额定容量的50%-40℃时以0.15C恒压2.66V/单体充电20h,再次放电容量为额定容量的35%

     2、常温(25℃±3℃)充电以0.1C~0.25C的电流恒压2.4V/单体充电12h24h,完全放电后即亏点后快充:以0.6CA~0.8CA

            的电流,恒压2.67V/单体充电2h,可获得80%以上的额定容量,目前公司还没有配套合作厂家的充电器提供,可以提供正常充电和快充模式的充电参数。