This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ769142: DASTATUS6() 庫倫讀取問題

Part Number: BQ769142


您好

想請教BQ769142 的庫倫讀取功能,UseA 使用1mA,

1. Current sense resistors 使用 2 mΩ,

使用充放電機台對電池進行放電,放電累積庫倫與 DASTATUS6() 讀取後累積計算值相當,

2. Current sense resistors 使用 1 mΩ,

相同條件使用充放電機台對電池進行放電,放電累積庫倫與 DASTATUS6() 讀取後累積計算值2倍,

想詢問使用不同Current sense resistors在設定上需要做調整嗎?

感謝