This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895M: Cold,hot temperature threshold问题

Part Number: BQ25895M


关于规格书上V(LTF)和V(HTF)阈值有点不太明白,比如V(LTF)BUCK MODE模式写的是TS PIN VOLTAGE  rising threshold是 V(REGN)的72.75~73.75,那假如REGN脚是6V,6X72.75%=4.365,6X73.75%=4.425,假如TS脚电压处于4.365~4.425之间则表示电池处于V(LTF)模式?还是当TS脚电压大于4.365或4.425才是处于V(LTF) cold模式?同样道理V(HTF) HOT模式TS PIN Voltage rising threshold是V(REGN)的47.75%~48.75%, 6X47.75%=2.865V,6X48.75%=2.925V,当TS脚电压在2.865~2.925之间是hot mode?还是大于2.925才是HOT MODE?最后一个问题 V(TCO) CUT-OFF temperature是指什么CUT-OFF的电压?