采用BQ40z50-R1做3S1P项目,目前采用0.2c做golden更新成功,RSOC没有跳变,只是更新出来的FCC比实际放出的实际容量小些,一般更新出来会比实际大些,目前在刚开始充电的时候RSOC会从0%跳2,之后充电过程无跳变,放电过程也正常,无跳变,就是刚开始充电的时候RSOC会从0%跳2,不知道什么原因?以下为数据截图,和设置参数,麻烦大神帮忙看下,如何解决?谢谢!3S.gg.csv7652.验证数据.xls
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用BQ40z50-R1做3S1P项目,目前采用0.2c做golden更新成功,RSOC没有跳变,只是更新出来的FCC比实际放出的实际容量小些,一般更新出来会比实际大些,目前在刚开始充电的时候RSOC会从0%跳2,之后充电过程无跳变,放电过程也正常,无跳变,就是刚开始充电的时候RSOC会从0%跳2,不知道什么原因?以下为数据截图,和设置参数,麻烦大神帮忙看下,如何解决?谢谢!3S.gg.csv7652.验证数据.xls
不好意思,验证第一个循环时充电是没问题的,看现象是做了大电流放电后(大于0.5c)后充电就会有跳变
您好,将smooth功能使能改善RSOC充电时跳变问题。
[SMOOTH]: A change in temperature or current rate can cause a significant change in Remaining Capacity (RemCap) and Full Charge Capacity (FCC), resulting in a jump or drop in the Relative State-ofCharge (RSOC). This function provides an option to prevent an RSOC jump or drop during charge and discharge.
您好,I jump of 2% during start of charge seems like a minor issue, I suspect this may be related to gauge re-running a capacity calculation at the start of charge which can cause a small jump in FCC/RemCap, or depending on the setting of relax_smooth_OK and relax_jump_OK could be part of their expected behavior.
您好,和我猜想的一致,但是客户不允许这个0跳2的跳变,目前验证数据relax_smooth_OK 设置的是1, relax_jump_OK设置的是0,目前如何调整可以解决这个跳变?谢谢!
您好,One of the only other bits I could see having an impact on this behavior is the LOCK0 bit which they have set. At the start of charge the LOCK0 is cleared and may be causing the small jump. Please disable this bit.
我做了不同实验,放电完后(放电电流大于0.5c),静置时间越长,刚开始充电跳变量越大,这个问题不知道怎么解决?客户使用放电电流是大于1c的,谢谢!
4.5A验证数据.xls0820.3S.gg.csv以上为验证数据和设置的GG文件,目前看放空后,静置时间越长,刚开始充电时跳变越大,不一定是0跳2,放空静置半小时,刚充电,,RSOC,0会跳到8,不知道怎么解这个问题,客户是不允许跳变的
您好,您发的数据没有跳变到8的数据,
目前看放空后,静置时间越长,刚开始充电时跳变越大,不一定是0跳2,放空静置半小时,刚充电,,RSOC,0会跳到8
这部分数据能发过来一下吗?
您好,I was looking through the data shared, I'm not sure what has happened from the previous discharges, but it looks like you may be able to reduce the jump by using a different load select setting. Also, do not test a constant current discharge with load mode = 1, this causes the gauge to think more current will be applied later in the discharge since it is simulating with constant power and will cause miscalculation in capacity which will lead to RemCap/FCC jumps
我目前设置Load Select为3,Load Mode为1,对于负载模式我试过Load Select为7,Load Mode为1,没有改善效果,根据我这项目实际的情况能推荐合适的Load Select和Load Mode值吗?我这边可以验证,谢谢!
您好,It will not matter which load select you set if the load mode = 1, the simulation expectations do not match the actual load so accuracy will be impacted.
3S-BQ40Z50R1验证-.xlsload mode = 0,Load Select=3不变,目前验证,放空还是静置10分钟,刚开始充电,还是会有0跳2的跳变,这是详细数据,不知道怎么解决这个问题了