This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61048: 2.4-4.2V的输入电压,转换到4V,是否可以使用2.2uH的电感?

Part Number: TLV61048


    规格书中提供了2个示例,输出电压是12V和14V,使用的是4.7uH的电感,输出电压降低,也就是压差降低,是否可以使用更小的电感?如使用2.2uH的电感。

谢谢!