Other Parts Discussed in Thread: USB-TO-GPIO2,
你好,TI的FAE技术支者大咖,本人由于电池管理项目需求带主动均衡,目前TI只有这款BQ78PL116电池管理芯片能满足需求,在官网不能下单买到USB-TO-GPIO2这个工具吗?如果实在没有,自己只能利用开源的原理图自己设计一下,但这个USB-TO-GPIO2的固件可以提供一份吗?这个固件能支持BQ78PL116即可。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,TI的FAE技术支者大咖,本人由于电池管理项目需求带主动均衡,目前TI只有这款BQ78PL116电池管理芯片能满足需求,在官网不能下单买到USB-TO-GPIO2这个工具吗?如果实在没有,自己只能利用开源的原理图自己设计一下,但这个USB-TO-GPIO2的固件可以提供一份吗?这个固件能支持BQ78PL116即可。谢谢!
您好,两个区别如下:
The USB-TO-GPIO2 uses a different core processor than the USB-TO-GPIO. This provides the USB-TO-GPIO2 with a range of improved functionalities that include BUS monitoring, 1MHz clock speed support, on-board burst and script modes we well as others.
The USB-TO-GPIO2 uses a different interface API than the USB-TO-GPIO, so it will require the latest version of the GUI software to recognize and interface with it.
这款芯片不推荐在新设计中, it is not the best device to select since the product is very old and the engineers familiar with the device are no longer around, so support will be limited.