Other Parts Discussed in Thread: EV2400, BQ4050
BQ25798项目中,出现一个异常的情况,Vsys输出正常,但BAT引脚输出电压却是异常的,具体情况如下:
BQ25798的电池包处于关机状态,即电池包没有输出了。BQ25798的VBUS输入16V,此时,用万能表测量Vsys电压,有12V,BQ25798设置的Vsys最小也是12V,这是正确的。但,奇怪的是,万能表
测量BAT引脚时,BAT引脚的电压只有2.1V,BQ25798的状态LED灯也是常亮,根据bq25798规格书说明,LED常亮表示在充电,但实际上,电池包并没有冲电。
然后通过EV2400来观看BQ25798的状态,也是显示正常充电,没有发现警报。
电池包用的芯片是BQ4050,根据BQ4050规格书来看,在shutdown模式下,只有pack有冲电电压,bq4050就从shutdown模式返回到正常模式。
电池包为4S。
请问为什么会出现BAT输出的充电电压只有2.1V,远远低于16.8V,而充电状态又没有警报?