This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,感谢回复,我们是采用280049C来进行控制的,但由于资源不够,所以无法给副边的开关管驱动信号。下面我给出了我们拓扑的一个示意,因为需要减小导通电阻,因此副边采用了两个低侧开关管并联,用一个UCC24612进行驱动。现在系统输入电压为18-36V,变压器匝数比为2:5,但输出电压为21-36V,比芯片规定的VDD28V要高,因此我按照datasheet中的典型电路,在VDD与REG之间并联了一个27V的稳压管,并且设计了一下限流电阻为1K。总结有两个问题:
一是在UCC24612驱动电流够的情况下,驱动两个并联的管子可行吗?
二是由于输出电压高于芯片耐压,但不多,用一个稳压管进行供电可行吗?