This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21530: 高压无法输出完全的低电平

Part Number: UCC21530


 比如高压输出400V,JP3的1号脚可以到400V,但是无法到0V只能到10.8V,请问有改进的方法吗?频率1Hz