This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: TPS25750DRJKR+BQ25792 充电问题

Part Number: TPS25750


1.插上传统充电器5V 2.5A 给机器充电,有时充电电流为500ma,有时为1.5A,INT现象,我硬件上断开
TPS25750 GPIO4 GPIO5线路,充电电流稳定在1.5A,我们GPIO如图使用的默认配置,
请问我们应该怎么设置GPIO配置,实现BC1.2充电,目前PD充电正常。

  • Hi

        建议你将这个问题放到美国E2E上,这个芯片只要是程序控制,结合其他芯片一起使用,我这边没有这个芯片的控制例程之类的文档。

        美国E2D上有这个芯片产品线的工程师,他们更加熟悉这个芯片方案的控制,也可能有例程之类的文档。