Other Parts Discussed in Thread: TPS61040
TPS61040-Q1 这颗料,我们发现,当负载比较低的时候(小于10mA不到负责时),PFM模式下震荡很厉害,如下图,不知道有什么好的方式,可以让信号减少震荡?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS61040-Q1 这颗料,我们发现,当负载比较低的时候(小于10mA不到负责时),PFM模式下震荡很厉害,如下图,不知道有什么好的方式,可以让信号减少震荡?
Hi
你是指上述SW波形吗? 如果是这样的话,是正常的,芯片这样是因为可以提高轻载效率。
您好,我是使用这颗料的客户,上图是我们测试的情况,
因为我们的负载确实很低,PFM模式下,SW信号振铃比较大,工作频率在150-180K左右,但现在有个问题,我EMC中RE辐射这个频率段FAIL掉了。超了10多个db;
1)想问您有什么好的建议吗?
2)我们现在整改,给输出加了1K左右的下拉电阻,这样让其工作模式进入连续工作模式,就想避免这个频率出问题,但又伴随另一个问题,工作频率由150K左右转移到了800K左右,我们担心两个问题a)这样增大其输出功率是否由影响b)这样800K频率段,我们可能会FAIL掉,所有我们想如何不改变其工作频率的状态下,去优化这个电路设计,让我们的EMC顺利PASS?
是的,SW波形;LIN XUE是使用这颗料的客户,但是有些问题,他在下面描述了,能否帮忙解答下,谢谢