This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430 12V降到5V,但是实际上输出电压低的问题



1.问题描述:zi lin Li 提出问题:

用的是官网上的原理图,第一次出来有5.76V,然后换了个电感,因为C3电容耐压值没选大一点,爆了,然后换了个耐压更高的电容,然后就输出电压1.1V左右,1脚9V,8脚0.2V,稳压管两端电压0.6V,4脚电压才0.24V左右,按照公式来算输出确实是1.1V左右,但是4脚基准电压有1.221V,低了很多,不知道怎么回事

2.原文链接:http://www.deyisupport.com/question_answer/analog/power_management/f/24/t/67734.aspx

3.解答问题的TI FAE: tao smith

4.个人的收获:

按照原帖楼主的设计参数,我用TI仿真工具进行了下仿真,大致过程如下: