如上图所示:
VIN=12~17.6V
VOUT=19.2V
当我的TPS61178正常工作,在TO_LINK_DCIN端加20V,就会导致IC烧毁,请问这是什么原因?我要怎么避免,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如上图所示:
VIN=12~17.6V
VOUT=19.2V
当我的TPS61178正常工作,在TO_LINK_DCIN端加20V,就会导致IC烧毁,请问这是什么原因?我要怎么避免,谢谢!
Hi
芯片输出有二极管PD703阻断,如果你是在TO_LINK_DCIN端加20V, 20V电压不应该 会流向芯片,你需要再确认一下是否是因为增加电压导致芯片损坏的。
如果确认有损坏的话,20V通过二极管给到输出,是否还会损坏芯片?
1.SW对地,很容易烧毁,像是下管烧掉了
2.增加电压是指增加TO_LINK_DCIN还是BOOST的电压?
3.另外该IC输出19.2V是否有risk,是否是SW的电压比较大导致下管烧掉?
4.另外线路能帮忙check一下吗?