Other Parts Discussed in Thread: ADS1247
这个是我曾经发的一个技术问题贴:求推荐配套ADS1247芯片的电压参考源?
地址链接:
http://www.deyisupport.com/question_answer/analog/data_converters/f/58/t/48231.aspx
问题是这样的:当时打算用ADS1247芯片进行小信号(0-20mV)采集 ,工作电压5V,为避免干扰,不想采用
运放进行信号放大,而是想直接进行采集,请问TI专家,在利用ADS1247设计电路时应该注意哪些方面呢?还有,能不能帮忙推荐一款TI的电压基准芯片呢?非常感谢!另外,不知道REF5020能否满足要求呢?
真是非常感谢四位TI专家Johnsin Tao、Van Yang、Carter Liu和 Kailyn Chen的热心回复:在他们的启发下,我逐渐熟悉了ADS1247这颗芯片,并明白了在用24位芯片做到20位左右精度的情况下,不用外部运放是不行的,采用的电压参考源REF5025芯片 要好于REF5020芯片,并同时也找到了一个合适的运放芯片,最终实现了一个19位的精度,在不增加成本的情况下,这样就能满足要求了!
小信号采集是一个比较棘手的问题,提高精度确实费工夫,真心感谢4位专家的热心指导!祝福他们工作顺利!越来越好!