This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25887: BQ25887配置使用?

Part Number: BQ25887


当前在安卓13的XBL阶段样机启动需要读取电池电压,采用如下流程:

读取单节电池电压,在调试中发现,如果充电器插入状态下可正常获取电池电压,如果没插充电器则无法获得。这样的话无法根据开机电压来判断是否可以开机。

未充电状态下如何获得电池电压,需要哪些设置,请麻烦确认一下,谢谢!

  • 您好,正在询问更了解这款芯片的TI工程师,稍后回复。

  • 您好,请参考下面内容

    You would need to disable the Watchdog and Enable the ADC. Please read Section 8.3.5, "To enable the ADC, the ADC_EN bit must be set to ‘1’. The ADC is allowed to operate if either the VVBUS>VVBUS_UVLO_RISING or VBAT>VBAT_UVLO_RISING is valid. If no adapter is present, and the VBAT is less than VBAT_UVLO_RISING, the device will not perform an ADC measurement, nor update the ADC read-back values in REG17 through REG24."