This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: TPS61022的最大带载能力

Part Number: TPS61022

我们常规供电时5V,但供电电源会存在偶尔跌落到2V,持续时间40ms的故障,我们期望我们加入tps61022之后,能起到防止系统因为供电不稳导致系统重启的问题,我们系统的功率常规时15W,最大25W。

如果采用TPS61022,能否满足设计需求?

  • Hi

        你的需求是最大25W, 如果是5V电压拉低跌落到2V, 那么输入电流就会在15A左右,很难找到合适的芯片,TPS61022就不合适了。

        所以实际上你需要考虑的是如果降低电压的跌落,例如如果加大电容是的最大跌落会到3V, 那么电流就最大10A左右,如果能控制跌落到4V可以选择的芯片就很多了。

  • 我的跌落是一个瞬时过程,最大持续40ms的时间,也不能承受么?TPS61022最大能承受的输入电流是多少?是ILIM_SW min6.5A,typ8A, MAX10A,也可以理解最大瞬时输入电流要控制在10A以内?

  • HI

        建议你通过波形来确认,我上面是考虑最差的情况,但实际上要尽量避免上述提到的电压跌落,除了加大电容外,还有加快反馈瞬态响应速度。

        对于你选择的DC/DC而言,同样需要考虑最恶劣的情况,有瞬态的大电流都有烧坏芯片的风险需要避免。TPS61022最大能承受的输入电流也需要考虑最恶劣的情况,所以是6.5A.

  • 前级电源是一个标准的电源板卡

  • HI

       也就是说没法加电容,那就再5V输出处增加一个大电容看看。

x 出现错误。请重试或与管理员联系。