我们常规供电时5V,但供电电源会存在偶尔跌落到2V,持续时间40ms的故障,我们期望我们加入tps61022之后,能起到防止系统因为供电不稳导致系统重启的问题,我们系统的功率常规时15W,最大25W。
如果采用TPS61022,能否满足设计需求?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你的需求是最大25W, 如果是5V电压拉低跌落到2V, 那么输入电流就会在15A左右,很难找到合适的芯片,TPS61022就不合适了。
所以实际上你需要考虑的是如果降低电压的跌落,例如如果加大电容是的最大跌落会到3V, 那么电流就最大10A左右,如果能控制跌落到4V可以选择的芯片就很多了。
HI
建议你通过波形来确认,我上面是考虑最差的情况,但实际上要尽量避免上述提到的电压跌落,除了加大电容外,还有加快反馈瞬态响应速度。
对于你选择的DC/DC而言,同样需要考虑最恶劣的情况,有瞬态的大电流都有烧坏芯片的风险需要避免。TPS61022最大能承受的输入电流也需要考虑最恶劣的情况,所以是6.5A.