This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: 关于TPS51200的EN管脚如何设计?

Part Number: TPS51200


我需要设计一块FPGA单板,上面会用到4颗DDR4芯片,上一个版本我使用了普通的LDO,在实际测试中VTT电压会升高到0.67V左右,猜测是由于需要灌电流引起的?

所以这次想使用TPS51200来给VTT提供电源。但是我看参考设计中EN都接到了SLP_S3,我并没有这个信号。如果我把EN直接上拉接到VIN,TPS51200跟普通的LDO还有区别吗?

规格书中的参考设计,Figure 31 中DDR3 Tracking Configuation的EN是直接接到Vin的,它跟接到SLP_S3有区别吗?